Issue
Clarification is required on the appropriate cable types to use for MicroNet LAN communications to ensure reliable and compliant system performance.
Product Line
Satchwell MicroNetEnvironment
Satchwell MicroNet
Cause
Selecting the correct communication cable is critical for maintaining signal integrity and ensuring proper operation of the MicroNet LAN. Using incorrect cabling may result in communication failures or degraded performance.
Resolution
For optimal performance and compliance with MicroNet LAN communication standards, the following cable specifications are recommended:
-
Standard One-Pair Communications:
Use Belden 8762 or an equivalent cable.- Belden 8762 is a shielded, twisted pair cable suitable for general communication wiring.
-
Isolated LAN Communications:
Use Belden 9502 or an equivalent cable.- Belden 9502 is a shielded, twisted pair cable designed for applications requiring electrical isolation.
📎 Attachments:
Additional Information:
- Always ensure that the selected cable meets or exceeds the specifications of the recommended Belden models.
- Proper installation practices, including grounding and shielding, are essential for optimal communication performance.