Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Using the V321 3-port globe valve, or similar, in a diverting application.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Using the V321 3-port globe valve, or similar, in a diverting application.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Product_Support
    Product_Support
  • sesa125819
    sesa125819

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3654 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Using the V321 3-port globe valve, or similar, in a diverting application.

Picard Product_Support
‎2018-09-10 12:25 AM

Issue

The V321 globe valve is described as a "Mixing valve", but  a diverting application is required.

Environment

Valves

Actuators

Diverting application.

V321

VTRE

Cause

The incorrect positioning of the V321 globe valve in the flow pipe work will lead to water hammer. Water hammer can lead to bad vibration and potential damage to the valve and pipe work.

Resolution

The V321 is a globe valve, and this style of valve must be fitted so that the water flows proportionally across the valve seats. This is achieved when the valve is fitted into the system return pipe work.

In the above drawing, it can be seen that the valve is fitted in the system return with its common port (AB) connected directly to the main system. Port A of the valve is connected to the heat load, and port B of the valve is connected to the bypass connection. This means that water will flow through ports A - AB if the valve is open, of ports B - AB if the valve is closed.

I must fit my valve in the system flow, what can I do?

If the valve must be located in the system flow, then this valve type is not suitable, and a different valve must be chosen.

The most logical choice of valve suitable for location in either the flow or return is the VTRE

It must be noted that this valve only has a rating of PN6 as opposed to the V321 which is rated PN16.

For the VTRE data sheet please click HERE.

Suitable actuators for the VTRE are either the M9B or EM9.

For the data sheet for the 24 volt / 230 volt M9B click HERE.

For the data sheet for the 0-10v DC EM9 click HERE.

Labels (1)
Labels:
  • Field Devices
Attachments
Tags (1)
  • Find more articles tagged with:
  • 5736
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.