Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Using a 4-20 mA CO2 sensor with a Xenta 102-AX in StruxureWare

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Using a 4-20 mA CO2 sensor with a Xenta 102-AX in StruxureWare
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • CraigEl
    CraigEl
  • Trey_Boothe
    Trey_Boothe
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2112 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Using a 4-20 mA CO2 sensor with a Xenta 102-AX in StruxureWare

Picard Product_Support
‎2018-09-10 09:50 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-14 10:01 PM

Issue

Configuring the Xenta 102-AX to accept a 4-20 mA CO2 sensor input on Universal Input 3.  A negative value is required on the CO2 offset value, but it is not possible to edit the scaling of the input in StruxureWare.

Product Line

EcoStruxure Building Operation

Environment

Xenta 102-AX

4-20 mA output CO2 sensor

SmartStruxure

Cause

The Xenta 102-AX universal inputs are designed to work with a 0-5V input.  The best option is to always buy a CO2 sensor that is compatible.  However, if 4-20 mA CO2 sensors have already been purchased and installed, they can be made to work.

Resolution

In this example, a 4-20 mA CO2 sensor with a 0-2000 ppm range is assumed.

  1. In the Xenta 102-AX Plug-In > Hardware Configuration Tab, set Input 3 Selection to None
  2. Wire the CO2 sensor and a 250Ω resistor across U3 and M.  This converts the 4-20 mA signal to 1-5V.
  3. In SBO WorkStation, create a Function Block program to convert the 0 to 100 % signal to ppm.  (You can import the Function Block program here).
  4. Edit Bindings on the CO2 Curve program and bind the nvoUnvInput3/Value.lev_percent from the UnivIn3Sense folder of the 102-AX to the CO2_RAW of the CO2 Curve program.
  5. Bind the CO2 from the CO2 Curve program to nviCO2/Value.ppm that is in the UnivIn3Sense folder of the 102-AX.

At this point, if you have values entered in for the Airflow Reset or CO2 Low Limit and CO2 High Limit then the Airflow reset will be active and operational.

Also, if you have multiple CO2 sensors on multiple 102-AXs then you don't have to have a CO2 Curve Function Block program for each one.  You can just edit the existing CO2 Curve program and copy/paste the exiting Function Block program multiple times in the same Function Block program.  You would just need to rename each public point with a unique name. 

Note: An input of 0V (a sensor that has not been wired yet) will result in an nvoCO2sensor value of 65535 (invalid).

Labels (1)
Labels:
  • EcoStruxure Building Operation
Attachments
Export CO2 Curve.zip
Tags (1)
  • Find more articles tagged with:
  • 19571
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.