Issue
- What is the Master to Slave controller ratio of Unifact Pro controllers on a LAN?
- What is the maximum number of Unifact Pro controllers on a LAN?
Product Line
Satchwell BAS & SigmaEnvironment
Unifact Pro
Cause
Clarification on:
- The ratio of Master to Slave controllers in a Unifact Pro setup.
- The maximum number of Unifact Pro controllers supported on a single LAN.
Resolution
-
Master-Slave Ratio:
➤ One Master controller can support up to three Slave controllers. -
LAN Capacity:
➤ A single Unifact Pro LAN can support up to 80 controllers in total. -
S-Link Sensor Sharing:
➤ An S-Link sensor wired to the Master controller can be shared by up to three Slave controllers.
➤ Important Note: If fan speed control is enabled, S-Link sensors cannot be used on Slave controllers.
Additional Resources 📎
- Download the Unifact Pro Datasheet
- Related documentation:
DS_13_303A.pdf