The difference between using "Control Output" and "Input Control Output"

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • The difference between using "Control Output" and "Input Control Output"
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • AdamSteele
    AdamSteele

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1606 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

The difference between using "Control Output" and "Input Control Output"

Guinan AdamSteele Guinan
‎2021-04-12 03:04 PM

Issue

When configuring an Input to control an Output in an Input Type, what are the differences between using the "Control Output" or "Input Control Output" options?

Product Line

EcoStruxure Security Expert

Environment

Security Expert

Cause

When configuring Input Types there can be some confusion with the terminology used to describe the two types of Outputs that can be controlled from an Input event. 

Control Output options on the Input Types Options (2) tabControl Output options on the Input Types Options (2) tabInput Control Output options on the Input Types Options (3) tabInput Control Output options on the Input Types Options (3) tab

Resolution

  1. The "Control Output" options refer to the Control Output defined in the Input Type's General tab.Control OutputControl Output
  2. The "Input Control Output" options refer to the Control Output defined in the individual Inputs General tab.Input Control OutputInput Control Output

An explanation for a related example would be:

  1. If a common output for all inputs of the Input Type then;
    1. On the Options (2) tab enable the Activate Control Output On Alarm and Deactivate Control Output On Restore.
    2. On the Configuration tab of the Input Type, set the Control Output to the output you want to trigger.
  2. Else if each input has a separate output then;
    1. On the Options (3) tab enable the Activate Input Control Output On Alarm and Deactivate Input Control Output On Restore.
    2. In each Input set the Control Output to the output you want to trigger.
Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (1)
  • Find more articles tagged with:
  • AdamSteele21
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.