Issue
The default Sigma user name TAC USER does not work with Sigma 4.05 SEB.
Product Line
Satchwell BAS & SigmaEnvironment
- Sigma 4.05 SEB
Cause
The default user name was updated starting from Sigma 4.05 SEB.
Resolution
From Sigma 4.05 SEB onwards, the default user name is:
SIGMA USER
(Note: The password remains unchanged.)
Additional Notes
- If login fails using
TAC USER, ensure the version is 4.05 SEB or later and useSIGMA USERinstead. - This change applies only from version 4.05 SEB onwards. Earlier versions still use
TAC USER.