Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Support for LON "File based CPT products"

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Support for LON "File based CPT products"
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Benji
    Benji
  • sesa125819
    sesa125819
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1334 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Support for LON "File based CPT products"

Picard Product_Support
‎2018-09-06 12:27 PM

Issue

Support for LON "File based CPT products"

Environment

LON

CP

CPT

SCPT

UCPT

Cause

Downloads / Uploads to the Roombox LON, and other "File based CPT products" fail.

Resolution

The Roombox controller uses the File based CPT's, and StruxureWare Building Operation does not support this, this means that uploads / downloads will always fail.

  • SCPT is an acronym for Standard Configuration Parameter (Types).
  • UCPT is an acronym for Used (defined) Configuration Parameter (Types).
  • CPT is an acronym for Configuration Parameters (Types). (Both SCPT and UCPT).

 

In the LonWorks technology it’s possible for the Vendor of the device, to implement these variables in three ways:

  1. As NV's (network variables)
  2. As “DMA type variables”, (meaning they just reside in the devices flash memory at known addresses)
  3. As “File Type” variables, (meaning they are located inside a logical file in the device)

 

StruxureWare Building Operation can handle type 1 and 2 above. But not type 3 at the current release (1.5)..

 

There is a fairly easy way to determine this, which is from the device’s XIF file.

If the XIF file contains these variables, (or at least the two first), then the SCPT's / UCPT's in this device ARE implemented as File type variables, and StruxureWare Building Operation can’t handle them.

  • nviFileReq
  • nvoFileStat
  • nviFilePos

Most of the devices having this, are using Loytec’s chip, so typically this can be: Lvis, Linx and many gateways from Loytec., but there are other products to. These devices are not easily commission in StruxureWare Building Operation.

However Product Support Services can assist you to edit the XIF file, so that the device can be commissioned.

Note - The SCPT's / UCPT's will be removed from the device, so these will not be visible (and of course not changeable) from StruxureWare Building Operation. Access to NV's will be as normal.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (1)
  • Find more articles tagged with:
  • 7745
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.