Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Steps to connect a 4-20mA or 0-20mA sensor to a Universal Input

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Steps to connect a 4-20mA or 0-20mA sensor to a Universal Input
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Ramaaly
    Ramaaly

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
7197 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Steps to connect a 4-20mA or 0-20mA sensor to a Universal Input

Picard Product_Support
‎2018-09-07 06:01 AM

Last Updated: Lt. Commander Ramaaly Lt. Commander ‎2025-09-03 11:08 AM

Issue

Current transducers require an additional external resistor fitting to a Universal input to read the current flow, what resistor and input point settings are required?

Product Line

Andover Continuum

Environment

  • All controller with Universal Inputs (both 5V and 10V).
  • 4-20 mA

Cause

There is a requirement to define the resistor value to be connected across the input, also the settings for the upper and lower voltage in the input point configuration.

Resolution

Download the attached Current Inputs.PDF file, although this was originally written for Infinity controllers it is fully applicable for i2 and b3 controllers. Controllers like the i2/b3920, i2/b3810 have 10V inputs other i2/b3 controllers have 5.12V inputs, check the product datasheet specification if you are unsure.

The file details the value of the resistor to use in the circuit and the upper and lower voltage settings to enter in the Auto Conversion box in the input point, these will correspond to the sensor reading at 0mA and 20mA, or 4mA and 20mA depending on your sensor output.

For controllers that allow the pull up resistor to be switched out, ensure that it is in circuit for these setting to work correctly.

The UI-8-10-10V I/O Modules should be set to 0-5V input with the reference resistor On, then setup as per all other 5.12V input controllers.

Note: The part numbers listed for the resistors are no longer available through Order Entry and should be sourced from your local stockist.

Link to file:

Current Input ISM.pdf

 

Suitable component resistors:

For 10V inputs: RS 165-472

For 5V inputs: RS 165-185

0

Labels (1)
Labels:
  • Andover Continuum
Attachments
Tags (2)
  • Find more articles tagged with:
  • 4450
  • RamaAly25
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.