Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

SpaceLogic BACnet/IP devices firmware compatibility with EBO and Tridium Niagara N4

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • SpaceLogic BACnet/IP devices firmware compatibility with EBO and Tridium Niagara N4
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RandyDavis
    RandyDavis
  • PeterEdvik
    PeterEdvik
  • Mahmoud_Sayed
    Mahmoud_Sayed

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
3 Likes
9951 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

SpaceLogic BACnet/IP devices firmware compatibility with EBO and Tridium Niagara N4

Mahmoud_Sayed Champion
‎2021-09-28 11:35 AM

Last Updated: RandyDavis Champion ‎2025-09-10 06:33 AM

Issue

What is the compatible SpaceLogic BACnet/IP device firmware version for my EBO or Tridium Niagara N4 installation?

Product Line

EcoStruxure Building Operation, TAC IA Series

Environment

  • SpaceLogic BACnet/IP devices
  • Tridium Niagara N4.10 and later versions Jace 8000/9000
  • Tridium Niagara N4.10 and later versions Enterprise Server 

Cause

The SpaceLogic (formerly known as SmartX) IP Controllers shipped from the factory may not have the latest firmware installed. It is essential to verify that the controller has the latest firmware build loaded for the EcoStruxure Building Operation version or Tridium Niagara N4 build being used before programming the controller.

Resolution

The below table contains the supported SpaceLogic BACnet/IP devices firmware for each EBO release. 

V7.00.0x compatibility.jpg
* CPs are available on: EBO Hotfix List
Note: Versions not mentioned in the table above are out of full support. Refer to earlier versions' release notes for the older versions' compatibility matrix, refer to EBO- Release Notes and Software Support Policy for EcoStruxure™ Building Operation  

Note: RP-C is only supported on EBO 3.0 and later

SpaceLogic/EasyLogic versions compatibility

MP-C-MP-V compatibility.jpg

SpaceLogic BACnet/IP devices can be upgraded using WorkStation, as explained in Updating Firmware in BACnet/IP Controllers. 

SpaceLogic BACnet/IP devices firmware can also be upgraded using the eCommission SmartX Controller mobile application, you can download firmware to either a single BACnet/IP controller or multiple controllers, even if not hosted. This is only supported over an IP connection, as explained in Using the eCommission SmartX Controller Mobile Application to Download Firmware to BACnet/IP Control...

 

Tridium Niagara N4 Compatibility

Note: Previous to Version 1.0, SpaceLogic BACnet/IP devices firmware is only approved at v3.02.03 for Jace 8000 and Niagara Enterprise Server using N4.10 and newer platforms.

Starting in Version 2.0 (Build 77) firmware v4.00.04.02002 CP1 is approved for use.  Make sure and reference the controller type in the table above as well. Release Notes 

Starting with Version 3.1 (Build 85), firmware 6.00.03.03007 CP2 and 7.x RC can be employed. The EasyLogic controllers are supported by the Niagara modules with these releases.  N4.10, 4.13, 4.14 and 4.15 are the only versions with these modules. Product Announcement  

 

 
Labels (2)
Labels:
  • Automated Engineering Tool
  • EcoStruxure Building Operation
Tags (5)
  • Find more articles tagged with:
  • MahmoudSayed21
  • MahmoudSayed22
  • MahmoudSayed23
  • MahmoudSayed24
  • MahmoudSayed25
Was this article helpful? Yes No
100% helpful (1/1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.