Issue
When attempting to shut down the PC, the Sigma SUM application prompts for a password to close.
Product Line
Satchwell BAS & SigmaEnvironment
Sigma SUM
Cause
Sigma SUM is designed to run continuously in the background. When the PC is shut down, the application requests a password to ensure controlled termination.
Resolution
To close the Sigma SUM application when prompted for a password, enter:
Password:
SUM
Additional Recommendation:
To avoid manual startup, add Sigma SUM to the PC’s startup programs so it launches automatically when the system boots.