Issue
When using Sigma on Windows 7, the holiday schedule dates do not fit properly within the display windows.
Product Line
Satchwell BAS & SigmaEnvironment
Sigma Client
Cause
The issue is caused by Windows 7 screen settings, specifically the default theme, which affects how Sigma renders its holiday schedule interface.
Resolution
This is considered a minor fault. A workaround is available:
To resolve the display issue:
- Right-click on the desktop.
- Select "Personalize".
- Scroll down and choose "Windows Classic" theme.
This change replicates the Windows XP display style, allowing the holiday schedule to render correctly.