Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Running I/NET Seven as a service on Windows

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Running I/NET Seven as a service on Windows
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4346 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Running I/NET Seven as a service on Windows

Product_Support
‎2018-09-07 12:15 AM

Last Updated: ContentModerator Explorer ‎2025-10-10 02:57 AM

Issue

Running I/NET Seven as a service on Windows

Product Line

TAC INET

Environment

  • I/NET Seven
  • All supported Operating Systems

Cause

When you log out of Microsoft Windows or restart the computer, all running processes are shut down. These processes are not resumed at log on or at restart. You have to start I/NET manually again. To get I/NET to start up when the computer restarts, you can run it as a service. Running a program as a service means that it runs in the background, but it is not visible on the Windows task bar.

Resolution

Use the INET Run Mode tool available on the Community.  Alternatively, you can perform the following steps to set/unset the InetIoSrv.exe as a service or application.

To register I/NET Seven to run as a service

  1. Open a Windows command prompt. Go to Start > Run and type "cmd"
    • Use right-click on the command prompt and select "Run as Administrator"
  2. Use commands cd.. (to go back one directory) and cd (to go into a folder) to navigate to the following location: C:\Program Files\INET Seven\
  3. If this is being run on a 64 Bit OS, the location then would be: C:\Program Files (x86)\INET Seven\
  4. Type the following command. This will unregister I/NET as an application
    inetiosrv /unregserver
  5. Type the following command. This will register I/NET to run as a Windows service
    inetiosrv /service
    CMDINETSeven.png

To verify the changes have taken effect

  1. Right-click on "My Computer" and select "Manage"
  2. Select Services and Applications > Services
  3. Look for Inet7Iosrv. It should be set to Automatic.

You are now running I/NET as a service. IOSrv will now be running in the background when the PC boots up. This does not require a Log On to the PC, however, you will have to Log On to the PC as a user to launch I/NET or AMT from the desktop icon. You will notice that IOSrv has been logging all AMT transactions, messages and alarms. The SQL Server and Agent were also running in the background receiving data to the database.

To set I/NET back to running as an application

  1. Open a Windows command prompt. Go to Start > Run and type "cmd"
    • Use right-click on the command prompt and select "Run as Administrator"
  2. Use commands cd.. (to go back one directory) and cd (to go into a folder) to navigate to the following location: C:\Program Files\INET Seven\
  3. Type the following command. This will unregister I/NET as a service
    inetiosrv /unregserver
  4. Type the following command. This will register I/NET to run as an application
    inetiosrv /regserver
    CMDREGServer.png
Labels (1)
Labels:
  • TAC INET
Tags (2)
  • Find more articles tagged with:
  • 2005
  • RobertAndriolo19
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.