Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Requirements for connecting Pelco's Endura to TAC I/NET Seven

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Requirements for connecting Pelco's Endura to TAC I/NET Seven
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • CraigEl
    CraigEl
  • sesa139513
    sesa139513
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
5831 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Requirements for connecting Pelco's Endura to TAC I/NET Seven

Picard Product_Support
‎2018-09-07 07:40 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-11 06:52 PM

Issue

The Pelco Endura system with cameras at a location and integrating with the TAC I/NET Seven system.

Product Line

TAC INET

Environment

Check the system requirements for the version of TAC I/NET Seven and Pelco Endura 

Cause

Configuration requirements of the Pelco Endura and TAC I/NET Seven are specific for the functionality in I/NET.

Resolution

Once your Pelco Endura system is configured and the Workstation has discovered all the devices and the System Manager is online with the cameras correctly configured, there are four basic requirements to connect TAC I/NET.

  1. Cameras have to have a unique friendly name other than default.
  2. Cameras have to have a unique camera number.
  3. Netframework 3.5 has to be installed.
  4. Windows Media Player 11 has to be installed.

 

If using I/NET Seven Release 2.40a then the following applies:
Once INET and the requirements above are installed the Endura Install can be run.
The installer for these files is located on the INET CD in the folder: Support\EnduraSDK.
Note: Endura video does NOT work on Windows Vista or Windows 7.
 
If using I/NET Seven Release 2.40 or above:
Dual NIC support is now available. For Endura, 100GB NIC and Router are suggested. 1 for I/O Server, 1  for video
 
Equipment used:
  • NSMS200 Pelco Endura Network System Manager & Network Video Manager
  • SM5000 Pelco Endura System Manager
  • WS5070 Pelco Endura Workstation with Advanced Management Software
  • WS5000 Pelco Endura Work Station Software package
  • NET5301T Pelco Endura Video Encoder
  • Spectra IV Pelco Camera

Visit Pelco.com for more information.

Click here to view an extended compatibility matrix for Endura and I/NET.

Labels (2)
Labels:
  • CCTV
  • TAC INET
Attachments
Tags (1)
  • Find more articles tagged with:
  • 4113
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.