Re-addressing I/A Series BACnet controllers on an existing BACnet MS/TP installation

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Re-addressing I/A Series BACnet controllers on an existing BACnet MS/TP installation
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RyanSuar
    RyanSuar
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2208 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Re-addressing I/A Series BACnet controllers on an existing BACnet MS/TP installation

Picard Product_Support
‎2018-09-10 04:53 AM

Issue

Re-addressing I/A Series BACnet controllers on an existing BACnet MS/TP installation

Environment

I/A Series R2 BACnet integration to I/A Series Micronet BACnet Controllers

Cause

There are gaps in BACnet MS/TP addressing which needs to be fixed. Gaps in addressing add delays in communications. Addressing should begin with node 0 (zero) and progress through all nodes, without any gaps, for each separate MS/TP
network.

Refer to the I/A Series MicroNet BACnet Wiring, Networking, and Best Practices Guide (F-27360-7).

Resolution

The procedure to change the addresses of the MNB controllers involves the following steps.

  1. Changing the physical DIP switch address on the MNB controllers.
  2. Making sure the MAC Address of the BACnet shadow device object in the I/A Series R2 UNC reflects the change.
  3. Changing the Max Master property in each MNB controller using WorkPlace Pro. Alternatively, you can change the Max Master property using the WorkPlace Commissioning Tool.

1. Changing the physical DIP switch address on the MNB controllers

  • Have a piece of paper ready to note down the physical DIP switch address before and after the change.
  • DIP switch addressing should be sequential starting from ‘0’ with no gaps in between. However, the physical location of the device does not matter. For example, if we have 30 MNB controllers on the BACnet MS/TP network, the addresses should be from 0 to 29 but they do not have to be in order physically. As an example, the first MS/TP device could have an address of '0' while the second MS/TP device on the wire can have an address of '10'. The MNB-1000 should be address ‘0’ if it is the first MS/TP device. If the first MS/TP device is an UNC, the UNC should be address '0' (set in WorkPlace Pro).
  • Use Table–2.3 to calculate the DIP switch value for physical addressing. Take, for example, that the address must be set to 16. To do so, you would set switch number 5 (value=16) to ON. If the address is to be set to 43, instead, you would set switches 1, 2, 4, and 6 to ON (value=1+2+8+32=43).

  • The controller should reset itself about 10 seconds after the change and the new address will be in effect.

2. Check / change the MAC Address of the BACnet shadow device object in the UNC using WorkPlace Pro.

  • After changing the physical DIP switch of the device, we will need to make sure that they change has been reflected in the corresponding BACnet shadow object device in the UNC.
  • Using WorkPlace Pro, open the UNC station.
  • Go to the Properties of the MNB shadow device object and go to the ‘Config’ tab.

  • Make sure that the 'MAC Address' field is showing the new address (in HEX) of the controller.

3. Changing the Max Master property in each MNB controller using WorkPlace Pro.

  • Each MNB controller under a particular BACnet MS/TP trunk needs to have their ‘Max Master’ setting changed. Set ‘Max Master’ to 1 or 2 higher than the highest address on the MS/TP network. If the highest addressed device is DIP switch value 50, set the Max Master to 51 or 52.
  • In WorkPlace Pro, open the UNC station.
  • Go to the Properties of the MNB shadow device object and go to the ‘Engineering’ tab.
  • Change the ‘maxMaster’ to a value that is 2 higher than the highest addresses device. Click ‘Apply’.
Labels (1)
Labels:
  • TAC IA Series
Tags (1)
  • Find more articles tagged with:
  • 6654
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.

You’ve reached the end of your document

WHAT’S NEXT?

Ask our Experts

Didn't find what you are looking for? Ask our experts!

My Dashboard

Check out the new Feeds and activities that are relevant to you.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.