Issue
A Niagara R2 UNC station fails to start and displays the following error in the Standard Output window:
FATAL: Cannot boot station from sns
java.lang.NoClassDefFoundError: tridium/foundation/prism/Subscription
Product Line
TAC IA SeriesEnvironment
R2 UNC
Cause
Resolution
To recover the UNC:
- Reinstall the operating system (OS) on the UNC.
- Reinstall the Niagara R2 runtime environment (NRE) and required modules.
- Restore or redeploy the station after the OS and NRE are successfully installed.