Issue
Users report that the Print option in the graphics menu is greyed out when logged into the system.
Product Line
Satchwell BAS & SigmaEnvironment
Satchwell Sigma Graphics
Cause
The issue occurs due to user account settings that do not permit print functionality while logged in.
Resolution
To resolve this issue:
- Access System Setup.
- Navigate to User Groups.
- Highlight the User Account experiencing the issue.
- In the Basic Settings section, enable the "Logged On" option.
✅ This change will activate the print functionality for all users associated with the selected account.