Issue
Product Line
TAC IA SeriesEnvironment
Niagara R2
Cause
routeAcks property set to True, which routes acknowledgment events to email recipients.Resolution
To prevent emails from being sent when alarms are acknowledged:
-
Open MailRecipient Configuration
- Navigate to the MailRecipient object in the Niagara R2 station.
-
Modify routeAcks Property
- Go to the Config tab.
- Set the
routeAcksproperty to False.
-
Apply Changes
- Click Apply to save the configuration.
After this change, acknowledgment events will no longer trigger email notifications.