Polling data over IP from the System pane of a 700 project

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Polling data over IP from the System pane of a 700 project
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Cody_Failinger
    Cody_Failinger
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1599 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Polling data over IP from the System pane of a 700 project

Picard Product_Support
‎2018-09-06 01:59 PM

Issue

Polling data from one Xenta Server to another can be accomplished over IP by importing XBuilder Projects. This will only bring over data points that reside in the Network Pane of the XBuilder Project.  If points are being calculated in a Menta object, for example, they would not be available following an import.

Product Line

TAC Vista

Environment

  • XBuilder
  • Xenta Server 701, 711, 721, 731
  • Fixing Write Over IP

Cause

Importing another projects network brings over only data points that reside in the Network Pane of the XBuilder Project. In order to avoid a write over IP situation, data from the System pane sometimes needs to be browsed into the other controller's project.

Resolution

  1. Expand the Network pane beneath the Xenta 700 and find the Variables folder.
  2. Right click on the Variables folder and select New Variable (if desired, choose New Folder to organize the points that need to be sent over IP).
  3. Create a variable for each point that needs to be imported into the receiving Xenta Server.
  4. Drag and drop Variables onto the Menta object outputs to associate them


     
  5. Note: Only Menta object Outputs allow for this drag-and-drop functionality.  If they are public signals, then either:
    1. Add an RO, IO, BO point on the output of the signal
    2. Use a connection object in XBuilder to transfer the value to the Network Pane variable.
  6. In the receiving controller's XBuilder project, right-click on the IP Backbone and select New > Other Projects Network.  Now the Menta object variables are available.
Labels (1)
Labels:
  • TAC Vista
Tags (1)
  • Find more articles tagged with:
  • 4946
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.