Issue
Users require access credentials to edit index or binary files within Doctor or SigmaX.
Product Line
Satchwell BAS & SigmaEnvironment
- BAS Doctor
- Sigma
- SigmaX Doctor
Cause
To perform modifications in Doctor or SigmaX, specific passwords are needed to unlock editing capabilities for index and binary files.
Resolution
To edit files in Doctor or SigmaX, use the following passwords:
- Index File Edit Password:
IE - Binary File Edit Password:
BE
🔹 These passwords are not case sensitive. You may use either uppercase (IE, BE) or lowercase (ie, be).