Issue
Product Line
TAC IA SeriesEnvironment
- Niagara R2
- Niagara G3
Cause
Resolution
- Overrides performed directly on the Block Output object are range-checked (valid range: 0–255).
- If using gxText or graphics:
- Add descriptive text or a warning near the override control indicating the valid range (0–255).
- Avoid entering values greater than 255 to prevent truncation.