Issue
A Niagara R2 Enterprise Server station fails to start. The Standard Output Window displays the following error:
ERROR: Cannot add key entry: 8390 java.lang.IllegalStateException: Missing class for: 24
Product Line
TAC IA SeriesEnvironment
Niagara R2 Enterprise Server station
Cause
Resolution
- Verify that all jar files in the station are part of the official Niagara R2 release.
- Remove any third-party or custom jar files that are not included in the standard installation package.
- Restart the Enterprise Server station after correcting the jar file set.