Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Modbus TCP Device (Slave) address greater than 247

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Modbus TCP Device (Slave) address greater than 247
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4577 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Modbus TCP Device (Slave) address greater than 247

Product_Support
‎2018-09-06 09:06 AM

Last Updated: ContentModerator Explorer ‎2025-08-11 03:56 AM

Issue

Modbus TCP Device (Slave) address greater than 247

Product Line

EcoStruxure Building Operation

Environment

  • Building Operation Enterprise Server
  • Building Operation Automation Server (AS, AS-P, AS-B) 
  • Modbus TCP Network
  • Modbus TCP Gateway

Cause

Modbus TCP Device (Slave) address 248 is reserved and cannot be used. (Modbus TCP Network or Gateway)

SmartStruxure supports up to address 247, as per StruxureWare Building Operation - Technical Reference Guide (up to v1.6.1).

There was a defect within v1.5.0 and earlier that caused address 250 to be used if the Device address is set to "Invalid." This defect was corrected in v1.6.1.

Resolution

From v1.9 this is corrected, so it is possible to define addresses for Modbus TCP devices from 1-247 and 249-254

Device addresses 0 and 248 are reserved.
Device address 255 is used as the Default address.

 

For Modbus RTU RS485 master/slave networks, slave device addressing is different, see KB article Modbus RTU slave address.

 

Further information about Modbus can be found in the KB article Modbus basics.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (5)
  • Find more articles tagged with:
  • 17666
  • 249-254
  • 26311
  • 676
  • DavidChild21
Was this article helpful? Yes No
50% helpful (1/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.