Issue
What is the maximum number of network variables that can be configured on Micronet ARCnet controllers?
Product Line
Satchwell MicroNetEnvironment
Micronet controllers, all variants.
Cause
This article provides general guidance on the limits of Network Variable Received (NVR) and Network Variable Transmitted (NVT) settings within Micronet ARCnet controllers.
Resolution
All Micronet ARCnet controllers support the following configuration limits:
- Network Variable Received (NVR): Up to 6
- Network Variable Transmitted (NVT): Up to 6
These limits apply across all controller variants within the Micronet ARCnet family.
For detailed engineering guidance and best practices, refer to the latest VisiSat Engineering Guide. This document includes comprehensive information on ARCnet configuration, controller setup, and network design considerations.
Refer to the VisiSat Engineering Guide for further information.