Menta public constants can only be used once

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Menta public constants can only be used once
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Jonas_Brissman
    Jonas_Brissman
  • DavidFisher
    DavidFisher
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1890 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Menta public constants can only be used once

Picard Product_Support
‎2018-09-10 12:43 AM

Last Updated: Janeway Jonas_Brissman Janeway ‎2024-08-22 02:15 AM

Issue

If a constant is set to public (meaning it can be edited by the user from the front end) then it can only be used once in a Menta application. Options > Constants Table will show you which constants are set to public. Any attempt to use them more than once will result in the following error:

Tam32
Public constant used more than once:

Product Line

EcoStruxure Building Operation

Environment

Building Operation Workstation

Cause

Typically a public constant is being used because the simplicity of a simple block is desired. A delay block may be used on three different fan commands and the user desires all of them to have the same delay attribute.

Resolution

To use one value for multiple simple blocks, the functionality of those simple blocks will have to be recreated using other Menta blocks until a single PVR can be sent to multiple HFBs. For example, instead of a delay block, some configuration of trigger and pulse blocks could delay the output and a PVR could be used to set the length of the delay.

Note: Non-public constants can be used multiple times in simple block parameters and expressions. For example, "pi" could be defined as 3.1415926535 and used in multiple equations. It's just public constants that cannot.

Labels (1)
Labels:
  • TAC Vista
Tags (2)
  • Find more articles tagged with:
  • 5861
  • JonasBrissman24
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.