Issue
What is the maximum number of site codes that can be loaded into a Continuum system?
Product Line
Andover Continuum
Environment
AC-1 and AC-1 Plus modules
Cause
Network design limitations
Resolution
There is no limit to the number of site codes that can be loaded in a Continuum system. However, each door can contain a maximum of four (4) site codes. In the case of an AC-1 module, if it loses communication with its associated Netcontroller, it will only allow access from the first two fields.