Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

MRs going to Sleep

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • MRs going to Sleep
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • sesa139513
    sesa139513
  • Roger_Bently
    Roger_Bently
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1589 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

MRs going to Sleep

Picard Product_Support
‎2018-09-06 03:09 PM

Issue

MRs going to Sleep

Environment

I/NET Seven site with MR's

Cause

When certain DDC Modules are being used in an MR it uses both the NOV RAM and RAM Memory

Resolution

When certain DDC Modules are being used in an MR it uses both the NOV RAM and RAM Memory.

When writing DDC care should be taken so as to not exceed the amount of memory that is within the device itself. It has 130 Bytes of RAM and 1024 Bytes of NOVRAM.

The MR supports six DDC module types and an interconnected control configuration up to 16, depending upon the types. It may appear that the memory is not maxed out, when it is all added up but it causes the MR to “go to sleep”. The user will have to go to the MCU Configuration and turn that MR Internal and then External again, to “wake it up”.

Depending upon the application, if there are more than 4 PID modules, the first 4 work, but the others do not.

This can also occur if there is a huge calculation on one of the points, the same symptom and result will apply. Please be selective as to which module and function you’re using for your application.

Note: MR-resident DDC modules only reside in the MR (not in the MCI, MRI or I/Site LAN. Therefore, these modules are not available for use in any MR tagged as Internal in the MCU configuration editor.)

The following table shows the amount of memory that each item uses:
 

  Points  
Point NOVRAM Bytes RAM Bytes
DI Point 4 1
DA Point 4 1
DM Point 4 1
DO Point (Internal) 4 1
DO Point (External) 4 3
DC Point (Internal) 4 1
DC Point (External) 4 3
AI Point (Internal) 16 3
AI Point (External) 16 5
AO Point (Internal) 16 3
AO Point (External) 16 5
PI Point 4 2
     
  Modules  
Module NOVRAM Bytes RAM Bytes
PID Module (Without Filter) 40 14
PID Module (With Filtering) 40 19
Floating Module (Without Filter) 40 12
Floating Module (With Filter) 40 17
Two Position Module (W F) 28 2
Two Position Module (W/O F) 28 7
Relay Module (Standard) 20 2
Relay Module (DBB, DBM, INT) 20 4
Reset Module 48 2
     
  Calculations  
Calculation NOVRAM Bytes RAM Bytes
Calculation Modules Overhead Module (fixed) 6 2
Each Operator (+, -, *, /, etc) 1 N/A
Each Point Address (P0, P1, etc) 2 N/A
Each Constant (C0, C1, etc) 4 N/A
Each Line (L0, L1, etc) 1 N/A
Calculation Module Total * 2
     
  Lines  
Lines NOVRAM Bytes RAM Bytes
MR-DDC Lines N/A 4

Note: Verify that you are using the most current EPROM for the revision of software that you are running.

Labels (1)
Labels:
  • TAC INET
Tags (1)
  • Find more articles tagged with:
  • 1843
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.