Issue
Users may encounter a Run-up/down influence node error when working with MN50 Controller Optimisers.
Product Line
Satchwell MicroNetEnvironment
Satchwell MicroNet 50 Series Controller
Cause
This issue is caused by a firmware limitation in earlier versions of the MN50 controller software.
Resolution
To resolve the error:
- Upgrade the MN50 Controller firmware to Version 5.02.
- This version includes a fix specifically addressing the Run-up/down influence node error.