Issue
Can the UPS option be added to an existing Continuum power supply?
Environment
Continuum Power Supply
PS120/240-AC85
Cause
Can the UPS option be added in the field to a Continuum PS120/240-AC85?
Resolution
No. There is no field upgrade kit to add the UPS option to a Continuum power supply.