Issue
Conflicts may arise when installing MicroNet View software alongside I/O server software from the provided disk.
Product Line
Satchwell MicroNetEnvironment
MicroNet View software with I/O server
Cause
MicroNet View includes built-in installation of the required I/O server software. Installing the I/O server software separately from its disk can lead to software conflicts.
Resolution
To ensure a successful installation:
-
Install Only MicroNet View Software
- Do not install the I/O server software from the disk supplied with the I/O server.
- MicroNet View automatically installs the necessary NCP/ARCnet or SNP I/O server components.
-
If Both Have Been Installed
- Uninstall all related software.
- Reinstall only the MicroNet View software.
Additional Notes
- This guidance applies to installations involving either NCP/ARCnet or SNP I/O servers.
- Reinstalling the I/O server software separately may result in communication issues or system instability.