We are pleased to announce the commencement of the Consumer/Home Owner Registration Process on Community. Consumers/Home Owners may now proceed to register by clicking on Login/Register. The process is straightforward and designed to be completed in just a few steps.

How to trigger an output when intercom is making a call

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • How to trigger an output when intercom is making a call
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • AdamSteele
    AdamSteele

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
1171 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to trigger an output when intercom is making a call

Guinan AdamSteele Guinan
‎2021-02-25 02:57 PM

Last Updated: Guinan RobertAndriolo Guinan ‎2021-02-25 02:57 PM

Issue

Require a relay contact to close when an intercom call is being made. The relay is then wired to an information display with displays to alert personnel of the incoming call. 

Product Line

EcoStruxure Security Expert

Environment

  • Security Expert
  • SX-IPI, SX-IPI-C

Cause

Require visual notification of incoming calls viewable by operators not currently at the monitoring desk.

Resolution

In the SP-IPI-C configuration settings, there are a number of options in the "Call State Trigger" setting that can be used to trigger the onboard output during certain conditions. One of these is when the intercom is making a call. 

  1. Under Security Settings, there is an option titled Alert Trigger Setting where the call state can trigger the output.
    Alert Trigger SettingAlert Trigger SettingCall State Trigger: enables the output to be triggered by the call state of the Intercom. The output triggers when the call state matches the selected state.
  1.  
  2. Enable the Call State Trigger and set the value to Calling or Ringing depending on if the SX-IPI-C is making or receiving the call.
    Call State TriggerCall State Trigger
    Wire the output relay into the SX-IPI-C input.
  3. Register the input with Security Expert. See details starting at the Adding the Expander Setup in the Security Expert system section in the SX-IPI-C IP Intercom with Camera Installation Manual.
  4. In Security Expert, configure the input to trigger an alarm which in turn will trigger an output.
    1. Create an Event Filter and add the following event type to it.
      1. Input <ZONE_NAME> Opened
    2. Create an Alarm
      1. add the Event Filter to it.
    3. Create an Area
      1. If you want a common output that triggers when any object alarms in that area then set the Alarm Output fields on the Outputs tab. If instead, you want the output tied to the Input Type or individual Inputs then go to the next step.
    4. In your Input on the Areas and Input Types tab add your Area to Area 1 field and set the Input Type 1 to Instant.
      1. In the options enable Log to Event Buffer so we can see the activations.
      2. If a common output for all inputs of the Input Type then;
        1. On the Options (2) tab enable the Activate Control Output On Alarm and Deactivate Control Output On Restore options.
        2. On the Configuration tab set the Control Output to the output you want to trigger.
      3. Else if each input has a separate output then;
        1. On the Options (3) tab enable the Activate Input Control Output On Alarm and Deactivate Input Control Output On Restore.
        2. In each Input set the Control Output to the output you want to trigger.

 

 

Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (1)
  • Find more articles tagged with:
  • AdamSteele21
Was this article helpful? Yes No
No ratings

Link copied. Please paste this link to share this article on your social media post.

You’ve reached the end of your document

WHAT’S NEXT?

Ask our Experts

Didn't find what you are looking for? Ask our experts!

My Dashboard

Check out the new Feeds and activities that are relevant to you.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.