Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

How to set up a door for keypad OR card validation

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to set up a door for keypad OR card validation
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Carl_Slack
    Carl_Slack
  • DavidFisher
    DavidFisher
  • Alan_Wood
    Alan_Wood
  • AbeMeran
    AbeMeran
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2333 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to set up a door for keypad OR card validation

Picard Product_Support
‎2018-09-06 02:54 PM

Issue

Sample Plain English program to set up a door to allow for either keypad OR card validation.

Environment

  • Continuum
  • Plain English
  • Infinity
  • NetController

Cause

Allowing the NetController to respond to a keypad as well as a card reader allows for flexibility in the security solution.

Resolution

How do I setup a door for keypad OR card validation

Create the following InfinityProgram in the NetController for each door. Change each program to the correct door name.

NOTE: If using this program, make sure that you do not have validate pin mode selected on the entry reader tab of the door editor.
--------------------------------------------------------------------------------------------------
'Looping, AutoStart Program

'Change officedoor to the name of your door
Watching:
IF officedoor\doorfault IS 2 THEN '0 for normal operation 2 if Fault (Tamper) detected
officedoor\entrynormmode = 8 'PINMode

officedoor\entrynocommmode = 8 'PINMode

GOTO Counting
ENDIF

Counting:
IF TS > 5 THEN 'Wait 5 seconds before switching back to SiteMode + CardMode
officedoor\entrynormmode = 3 'SiteMode + CardMode

officedoor\entrynocommmode = 3 'SiteMode + CardMode


GOTO Watching
ENDIF
---------------------------------------------------------------------
Press the # key once, it will place the door in PINMode (8) for the 5 seconds then back to SiteMode+CardMode (3).
--------------------------------------------------------------------------------------------------------
Here are the available EntryNormMode and ExitNormMode values

SiteMode = 1
CardMode = 2
GeneralMode = 4
PINMode = 8

If you plan to use more than one add the two numbers together (Example: SiteMode + CardMode + PinMode = 11)
------------------------------------------------------------------------------------------------------
Here are the available DoorFault values

1 = Database of doors, areas, and personnel is not functioning normally
2 = Entry Keypad is being tampered with
4 = Exit Keypad is being tampered with
8 = Entry Card Reader is being tampered with or has failed
16 = Exit Card Reader is being tampered with or has failed

---------------------------------------------------------------------------------------------------------
My Test case:

I created a person with a valid card and a valid PIN. When I used the card the door would open, after relock I pressed the # and immediately entered the PIN plus the #, the door unlocked.

If you have a door switch you could probably use it instead of the 5 second timer this would give you a little more control over the door so that the next person in line (with a card) would not have to wait.

CyberStation (v1.52.0.20021120)
NetController (v1.520010)
AC1 (v22)
HID ProxPro with Keypad

Note: this works on an ACX(5740/5720) also

IMPORTANT:

The sample PE program above only sets the EntryNormMode of the door. The program needs to set also the EntryNoCommMode and possibly the EntryNodataMode. If the door is a dual reader door then the corresponding attributes on the exit side of the door must also be set.

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 2770
Was this article helpful? Yes No
100% helpful (3/3)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.