Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

How to integrate Active Directory with Security Expert

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • How to integrate Active Directory with Security Expert
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • AdamSteele
    AdamSteele

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
1 Like
5448 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

How to integrate Active Directory with Security Expert

AdamSteele Champion
‎2019-06-13 06:57 PM

Issue

Understand methods for integrating Security Expert with Active Directory for creation and management of Operators and Users.

Product Line

EcoStruxure Security Expert

Environment

  • Security Expert
  • Active Directory
  • SX-AD-OPR
  • SX-AD-USR
  • SX-DB-SYNC
  • PowerShell

Cause

Security Expert Active Directory Integration provides synchronization and authentication for Active Directory users enabling organizations to leverage on the user management and security policies that Active Directory provides. This article looks at the details between each integration option.

Resolution

There are four options for Active Directory Integration.

1. Default Windows Authentication option.

  • This allows for logging in to Security Expert with the Windows User account credentials which could include AD users if on a Domain.
    • Operator object must be created in Security Expert and configuration of windows authentication option has some specific steps to be followed for it to work.
      Unable to login to Security Expert using Windows Authentication
    • Remember to use syntax "<domain>\<username>" for the username when configuring the Operator for a Windows user ON a  Domain.
    • Remember to use syntax "<computername>\<username>" for the username when configuring the Operator for a Windows user that is NOT on a Domain.
  • No extra license is required for this.

2. SX-AD-OPR : License for adding Security Expert Operators from AD.

  • Security Expert Operators will need to be added manually using the following steps:
    1. Navigate to Operators and click Add.
    2. Check the Windows Authentication box.
    3. Click the ellipsis adjacent to the User Name.
    4. Use the Active Directory Users window to search for the AD credentials you wish to use.
  • Once the Operator has been added, you may check the Windows Authentication option when logging in.

3. SX-AD-USR : License for adding Security Expert Users from AD.

  • This will allow an active directory domain windows group to be periodically polled for updates that will in turn update the Users in Security Expert.
    • Individual options for importing users, disabling user if AD user is disabled, disabling user if AD user is deleted.
    • Only user names are imported, other than this only action can be disabling of users in Security Expert. No other details can be updated or added.
  • See application note AN-141 Security Expert LDAP User Import Configuration.

4. SX-DB-SYNC : Data Sync Service with Powershell script.

  • Powershell script pulls user details out of AD and writes to a CSV file that the Data Sync Service then imports into Security Expert.
    • Can perform more functions than SX-AD-USR as any attribute from AD users can be mapped to any attribute in Security Expert users.
    • Will require powershell experience as the sample script may need to be modified.
  • See SEC-APP-03-1.0 – SX AD integration using PowerShell for a sample script and in-depth details on how to configure this solution for importing User data.
  • See SX-DB-SYNC Security Expert Data Sync Service Integration Guide for details on setting up and using the Data Sync Service. The guide is in the package ZIP file.
Labels (1)
Labels:
  • EcoStruxure Security Expert
Attachments
Tags (5)
  • Find more articles tagged with:
  • AdamSteele19
  • AdamSteele22
  • AdamSteele23
  • AdamSteele24
  • AdamSteele25
Was this article helpful? Yes No
100% helpful (3/3)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.