Issue
“Windows Shell Common DLL has stopped working.”
This prevents proper configuration of the tunnel client.
Product Line
TAC IA SeriesEnvironment
- I/A Series R2 LON Tunnel Client
- I/A Series R2 Serial Tunnel Client
Cause
Resolution
- Configure the Niagara Application Tunneling dialog box with the required station information:
- For Serial Tunnel: Select a valid COM port and enter host address, username, and password.
- For LON Tunnel: Select a valid LON port and enter host address, username, and password.
- Ensure the tunnel client is set to Silent Mode.
- Click OK to save the data.
- When the dialog box appears indicating Windows is checking for a solution, select Cancel before the timeout that prompts to “Close Program.”
- This action saves the station information successfully.
Note: This is a workaround for Windows 7 compatibility issues.