Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Entry PIN t/o message shown when using PIN PAD functions

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Entry PIN t/o message shown when using PIN PAD functions
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • sesa145087_brid
    sesa145087_brid
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1544 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Entry PIN t/o message shown when using PIN PAD functions

Picard Product_Support
‎2018-09-06 01:00 PM

Last Updated: Picard RobertAndriolo Picard ‎2019-06-27 03:09 AM

Issue

When using PIN code or PIN with card number for door entry, the door does not open. A time out message "Entry PIN t/o" is shown in AMT.

Product Line

TAC INET

Environment

  • I/NET
  • PIN Pad Reader

Cause

There may be two causes of this message:

  1. There is an output format for PIN Pad called burst format. There are several types of burst format available, for example 4 bit, 8 bit, 26 bit etc. For I/NET, it only accepts 8 bit and 26 bit type. If the burst format isn’t correct, there will be "Entry PIN t/o" message appeared, which means timeout for waiting for PIN entering.

  2. The digits of PIN are less than 6 bits.

Resolution

The following solutions are recommended for the two causes of this issue:

  1. For cause 1, the burst format of the PIN pad should be changed to 8 bit or 26 bit (Usually using 8 bit. If the extended PIN function is needed, 8 bit type should be chosen). For HID reader, there is a configuration card to change the burst format to specific type. Refer to HID relative documentation.
    NOTE: In most instances the Configuration Cards must be presented to the reader within 5 seconds of powering up the reader.

  2. For cause 2, if the digits of PIN are less than 6 bits, a "#" button needs to be pressed after entering the PIN. If this solution can't work, you can change the PIN to 6 digits by adding "0" ahead of the PIN. For example, the PIN is "3325", the PIN entered should be "003325".
Labels (1)
Labels:
  • TAC INET
Tags (2)
  • Find more articles tagged with:
  • 6726
  • RobertAndriolo19
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.