Issue
Product Line
TAC IA SeriesEnvironment
- I/A Series R2
- oBIX
Cause
Resolution
The web services license feature (webUi) is not required to run the oBIX service in an I/A Series R2 station.
However, the R2 license must include the obix feature for the service to function.
Example feature line in the R2 license:
features=coreRuntime;bacnet;lonworks;obix
If the license does not include the obix feature, the service will not operate.