Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Determining the MAC Address of a Tridium Jace

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Determining the MAC Address of a Tridium Jace
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RandyDavis
    RandyDavis
  • WaynePeters
    WaynePeters
  • sesa119747
    sesa119747
  • sesa116871
    sesa116871
  • sesa116868
    sesa116868
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3456 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Determining the MAC Address of a Tridium Jace

Picard Product_Support
‎2018-09-06 02:43 PM

Last Updated: Guinan RandyDavis Guinan ‎2024-06-10 10:11 AM

Issue

How the MAC address of an I/A Series R2 UNC, ENC, or a Jace 8000/9000 can be discovered

Product Line

TAC I/A Series

Environment

 I/A Series UNC (R2), ENC (AX), Jace 8000 and 9000 (N4)

Cause

Obtain the MAC address of the device for network configuration. 

Resolution

  1. The UNC-410 / 5x0 MAC address can be obtained in two ways:  Calculate the MAC using the serial number or use a command window on the connecting computer.
  2. Units built by Schneider-Electric have a serial number that ends in the letter B. If the UNC was built by Tridium (JACE), the MAC has a different prefix and it would be best to use the command window method.
  3. Example calculation: A UNC-510 with a serial number of 18496B -> 18496 converted to a hexadecimal value is 4840 hex -> add a 100 hex offset to the value -> 4940 hex.  Append a fixed prefix of 00-20-96-05 for al UNCs.  The MAC address for this UNC would be 00-20-96-05-49-40. This same calculation process applies to the ENC-410 and ENC-520 controllers that have a serial number ending with the letter B.
  4. Example calculation: ENC-520 with a serial number of 584520B -> 584520 converted to a hexadecimal value is 08EB48 hex -> add a 100 hex offset to the value -> 08EC48 hex.  Append a fixed prefix of 00-20-96 and the MAC address for this ENC would be 00-20-96-08-EC-48.
  5. The other method is to connect the computer and the UNC / ENC with a network patch cable, open a command window, ping the IP address of the UNC, and then use arp -a to display the IP and physical MAC address (NOTE: the arp command will only work over the network if the PC and the UNC / ENC are on the same IP subnet).
  6. The JACE-8000 uses a Mac address assigned by Texas Instruments. The MAC address cannot be determined without powering up the device. Once the device is powered and a platform connection is made you can find the Mac address under Platform/TCP IP configuration/Expand Interface 1 and 2, TCPPlat.png
  7. Calculate the MAC Address based on the serial number 
    *The first three bytes are 00:01:F0 which is Tridium's Organizationally Unique Identifier (OUI)
  8. JACE-9000 - the next three bytes are hex 96:40:00 + 2 times [the serial number minus 90000000] (in hex). That will give you the MAC of the second NIC. The MAC of the first NIC is that plus one. MACCal.png

     

    Note
    For OEM brand controllers the OUI may be different. You can search for an organization's registered OUI at IEEE.org
Labels (1)
Labels:
  • TAC IA Series
Tags (2)
  • Find more articles tagged with:
  • 3221
  • RandyDavis24
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.