Issue
Users require access credentials for IAC Touchscreen devices used in Satchnet IAC controller environments.
Product Line
Satchwell MicroNetEnvironment
Satchnet IAC controllers
Cause
Default passwords are needed to access various levels of functionality on the IAC Touchscreen. These credentials may be required during initial setup, troubleshooting, or reconfiguration.
Resolution
The default access levels and corresponding passwords are:
| Access Level | Default Password |
|---|---|
| Read Only | 1234 |
| Read/Write | 4321 |
| Super User | 1024 |
| ACK Alarm | 2513 |
🔒 Note: These passwords can be modified during programming.
🔍 To verify or change passwords, connect to the Touchscreen using VisiSat software and check the Properties section of the device.