Issue
What are the default access-level passwords for a MicroNet Touchscreen?
Product Line
Satchwell MicroNetEnvironment
MicroNet Touchscreen controllers
Cause
Default passwords are required to access various levels of functionality on the MicroNet Touchscreen. These passwords may be changed during system configuration.
Resolution
| Access Level | Default Password |
|---|---|
| Read Only | 1234 |
| Read/Write | 4321 |
| Super User | 1024 |
| ACK Alarm | 2513 |
🔧 Note: These passwords can be modified using VisiSat software. To view or change them, connect to the Touchscreen and check the password settings under its properties.