Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Creating an Extended Trend Log for b3 (Infinet i1/i2) Point and Value Logs

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Creating an Extended Trend Log for b3 (Infinet i1/i2) Point and Value Logs
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidChild
    DavidChild
  • Dave_Shore
    Dave_Shore
  • BillNeville
    BillNeville
  • Derrick_Ratliff
    Derrick_Ratliff
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2873 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Creating an Extended Trend Log for b3 (Infinet i1/i2) Point and Value Logs

Picard Product_Support
‎2018-09-06 10:34 AM

Last Updated: Dave_Shore Schneider Alumni (Retired) ‎2023-03-09 05:40 AM

Issue

Creating an Extended Trend Log for b3 (Infinet i1/i2) Point and Value Logs

Product Line

EcoStruxure Building Operation

Environment

  • b3 BACnet Controller
  • Infinet i1 & i2 Controller
  • Building Operation Automation Server, AS, ASP, ASB
  • Extended Trend Logs (ETLs)

Cause

Using an extended trend log to store log records for long periods of time. The extended trend log is often saved on a higher-level server with more storage capacity. This extra storage capacity enables the server to store more records before overwriting the old ones. For more information, see WebHelp. Configure extended trend logs for b3/i1/i2 devices the same way as configuring extended trend logs in other Building Operation devices. There is one difference, however. do not use smart logs when configuring extended trend logs in b3 BACnet devices. Instead of using smart logs, use the Maximum Transfer Interval property to specify the transfer interval.

Resolution

  1. In Listview, select the b3/Infinet Object (point or value), click Properties/Advanced
  2. Multiply the "Log records" by the "Log interval" to calculate the maximum transfer interval.
    The "maximum transfer interval" is the frequency at which the extended trend log will transfer log records from the b3/Infinet Object before any entries in the b3/Infinet controller log are overwritten
  3. Right click the object, choose New then "Extended Trend Log"
  4. In the Create Object box, set Smart Log to False, Set the "Maximum transfer interval" to less than that calculated above (2)
  5. Click Create

For Infinet systems always refer to Infinet under the hood otherwise the creation is as the Webhelp for creating BACnet B3 Logs
In theory it would be possible to create the Extended Trend Log in an ES (where there is more storage capacity), but this could introduce other timing and bandwidth issues, so it is usually best to keep the first Extended Trend Log in the AS, then extend this to a second Extended Trend Log in the ES, as shown. (the second ETL in the ES scan use smart logging in the usual way)

2023-03-09_13-38-41.jpg

If significant logging is required then External Log Storage should be considered. (the B3 or i1/i2 logs still need to be collected via Extended Trend Logs)

 

 

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (4)
  • Find more articles tagged with:
  • 12802
  • DavidShore19
  • DavidShore21
  • DavidShore23
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.