Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Configuring a Smart Sensor in SBO

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Configuring a Smart Sensor in SBO
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
4021 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Configuring a Smart Sensor in SBO

Picard Product_Support
‎2018-09-11 11:48 AM

Last Updated: Crewman ContentModerator ‎2025-08-11 03:55 AM

Issue

Configuring a Smart Sensor in SBO.

Product Line

EcoStruxure Building Operation

Environment

  • StruxureWare Building Operations
  • b3xxx Controllers
  • Smart Sensor (LCD or LED)

Cause

Unsure how to program for a Smart Sensor in SBO.

Resolution

Some considerations to be aware of first;

  1. Object naming differences
    Programming of the Smart Sensor is very similar to the old Plain English programming used in Continuum. One of the main differences is that each input must be specifically defined at the start of the program.
    Depending on the version of SBO, there may be some other considerations with setting up/reading the LcdDisplay array by renaming of the BACnet AnalogValue's to remove the "_AV" from the BACnet name. This naming issue affects SBO v1.4.
  2. Specific variables for Smart Sensor to be used in Plain English programming.
    Here is an old Smart Sensor Installation manual that will help explain which objects need to be created and how they work in the controller to enable the LCD display. Create the LCDDisplay and SpaceTempSP as numerics and any other objects that are not already created as InfinitySystemVariables. See "Configuration and Programming" section in the manual starting on page 14.
    Also note that the sensor will not light up until values are written to it.
  3. Sample Plain English code.
    LCDDisplay (or LEDDisplay) is not automatically created. Create this numeric and assign it as an array with 8-elements. 
    If it is an LCD Smart Sensor, then create a numeric and name it "LCDDisplay" and set its logsize to 7 (this configures it as an array with 8 elements from 0 to 7). If it is an LED Smart Sensor, then create a numeric called "LEDDisplay" instead.
    After creating this numeric you should be able to create the PE Program successfully. The simple program below will show the current spacetemp (LcdDisplay[1]) in two decimal place format (LcdDisplay[2]) when the Display key (LcdDisplay[0]) is pressed. The degrees symbol (LcdDisplay[7]) is also shown. Consult the Smart Sensor Installation and User Guide starting on page 16 for more details on how these values are configured.
    Numeric Input SpaceTemp
    Numeric Output LcdDisplay
    
    Initialise:
      LcdDisplay[2] = 0
      If LcdDisplay[0] = 4 then Goto ShowTemperature
    
    ShowTemperature:
      LcdDisplay[1] = SpaceTemp
      LcdDisplay[2] = 12
      LcdDisplay[7] = 1024
      If TS > 30 then Goto Initialise

In SBO, do the following under the Application section of the b3 controller:

  1. Create a BACnet Analog Value object in the b3 called "LCDDisplay".
  2. Go to the Advanced tab and under the Log Settings section change Log Records to be 7.
  3. Save the changes.
  4. Create the program and add the above PE Script.
  5. Add the binds to the LCDDisplay object created in step 1, RoomTemp input, and any other objects used in the program.
Labels (1)
Labels:
  • EcoStruxure Building Operation
Attachments
Tags (1)
  • Find more articles tagged with:
  • 14982
Was this article helpful? Yes No
100% helpful (2/2)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.