Changing a Doors Door Type based on Arm State of the Area

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Changing a Doors Door Type based on Arm State of the Area
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • AdamSteele
    AdamSteele
  • BillNeville
    BillNeville

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
1325 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Changing a Doors Door Type based on Arm State of the Area

Captain BillNeville Captain
‎2021-09-01 01:53 AM

Last Updated: Guinan AdamSteele Guinan ‎2021-09-09 02:21 AM

Issue

This is useful when you are disarming areas from a card reader as you can secure the disarming portion by requiring a PIN code, preventing somebody from using a lost or stolen card to disarm the area while maintaining the convenience of Card Only once disarming has occurred.

Product Line

Security Expert

Environment

  • Security Expert Client
  • Security Expert Server
  • SP-C-Web

Cause

Prevent someone from using a lost or stolen card to disarm an area while maintaining the convenience of Card Only once disarming has occurred.

Resolution

  1. Create a new Schedule (SX = Sites > Schedules, SPC-Web = Time > Schedules) with the following settings:
    1. Check/enable all days for Period 1, leave start and end times default so you are left with a 24/7 schedule
    2. Under Options enable 'Validate Schedule When Qualify Output is On', set the 'Qualify Output' to whatever output is configured as the Disarmed output for the required Area.
    3. If you aren’t using a disarmed output currently you will need to assign one, this can be a Virtual Output if you do not want to use a physical output.
  2. Create a new Door Type (Programming > Door Types) with the following settings:
    1. Operating Schedule = The schedule from Step 1
    2. Secondary Door Type = The default Card AND PIN door type created by the system
    3. Entry Reading Mode = Card Only
    4. Exit Reading Mode = Card Only
  3. Locate the required Door(s) (Programming > Doors) and change the Door Type to the one created in Step 2.

When the Area is disarmed the schedule will be valid so the Door Type will be Card only when the schedule is invalid (which will be whenever the area is armed as the disarmed output deactivates upon arming) the secondary door type of Card + PIN will be used.

You can use other combinations of Door Types as required

Labels (1)
Labels:
  • EcoStruxure Security Expert
Tags (1)
  • Find more articles tagged with:
  • BillNeville21
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.