Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

CSC - Help with checking the operation of this controller.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • CSC - Help with checking the operation of this controller.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2239 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

CSC - Help with checking the operation of this controller.

Picard Product_Support
‎2018-09-10 03:34 AM

Last Updated: Crewman ContentModerator ‎2025-10-10 02:54 AM

Issue

Checking operation of CSC.

Product Line

Field Devices

Environment

  • CSC5252
  • CSC5352

Cause

The operation of the CSC compensator explanation.

Resolution

The operation of a compensator is to adjust the system flow temperature, in relation to changes in the outside air temperature. The system flow temperature can be further adjusted by the addition of a room temperature sensor, which will provide room influence.

The CSC 5252/5352 controller is programmed with a complete set of "Default" settings, these settings will allow the controller to operate as soon as its powered up.

Although the controller has a complete range of adjustable settings, accessed through the "Fine Tune Mode", for a basic installation the "Quick Set Mode" can be used. The screen shot below explains how to enter the Quick Set Mode and the settings available.

Controller data sheet

Controller User guide

 

Compensated Flow Temperature Set-point:

The compensated flow temperature set-point is automatically adjusted based on a ratio for set-point adjustments against the outside temperature changes.

A consistent ratio across the entire outside temperature range, may not provide suitable control.
For example: with radiator type systems, radiators are less efficient at lower water flow temperatures and need to be provided with a higher temperature to compensate for this initially.

The “Set compensator ratio 1”and the “Set Ratio 2” settings provide the ratio of the change to the flow temperature set-point for changes in the outside air temperature, the ratio used is based on the “Set Change-over Value”, with the compensated slope starting from the “Set Flow Origin”.
The “Set Flow Temperature Set-up Value” and “Set Night Set Back Value” provide a constant adjustment of the flow temperature set-point to a given building control requirement.

The default settings would give a resultant flow temperature as shown follows:

 

Image 1.jpg

 

The CSC5352 Calculator presents these settings in a graphical and listed format, making it easier to visually confirm the effects any changes to these settings would make.

 

 

Labels (1)
Labels:
  • Field Devices
Attachments
Tags (2)
  • Find more articles tagged with:
  • 6296
  • GaryMontague21
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.