Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

BACnet Schedule goes into Fault and shows a value of "ConfigurationError" in its Reliability field.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • BACnet Schedule goes into Fault and shows a value of "ConfigurationError" in its Reliability field.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • JohnBoehmer
    JohnBoehmer
  • AbeMeran
    AbeMeran
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2053 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

BACnet Schedule goes into Fault and shows a value of "ConfigurationError" in its Reliability field.

Picard Product_Support
‎2018-09-06 02:00 PM

Issue

After configuring a BACnet Schedule in a BCX or a b3 controller, it goes into Fault with its Reliability field showing "ConfigurationError".

Environment

  • CyberStation
  • WebClient
  • BCX40xx
  • b3
  • BACnet Schedule Object

Cause

Configuration of BACnet schedule

Incorrect point type used to configure BACnet schedule

Resolution

For each object type within BACnet (input, numeric, trendlog, etc.) each object property identifier (property) has an associated data type.  A list of data types for the each property can be found in Chapter 12 of the BACnet spec under the section for each object type. 

The correct data type to configure in the schedule is determined by the Object property that is being controlled by the schedule object.  When using a schedule to control the value of a BinaryInput, BinaryOutput and BinaryValue objects, the Data Type that should be used is Enumerated.

When using a schedule to control the value of a AnalogInput, AnalogOutput and AnalogValue objects, the Data Type that should be used is Real.

When using a schedule to control the value of a MultiStateInput, MultiStateOutput and MultiStateValue objects, the Data Type that should be used is Unsigned Integer

The Schedule object can be tricky to configure, however. There are several properties (Weekly_Schedule, Exception_Schedule, Schedule_Default) that must contain the same data type for all events. Since Enumerated is the “default” data type, the user may need to manually remove any existing events with the Enumerated type and replace them with the desired data type.

If while configuring the schedule a message similar to the one above is displayed and accepted  all the events MUST be deleted otherwise a configuration error will result.

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 4897
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.