Issue
When viewing the alarm summary of an I/A Series R2 UNC through a browser, the alarm and alert counts display as unknown. Attempting to view alarm details generates the error:
The requested information could not be retrieved from the database.
Product Line
TAC IA SeriesEnvironment
I/A Series R2 UNC
Cause
Resolution
- Verify that the notification service archiveMode is set to:
archive_local_no_SQL - Reboot the UNC after making this change.
- Failure to reboot will result in the error persisting.