Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Access Expert Reader Troubleshooting

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Access Expert Reader Troubleshooting
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Alan_Wood
    Alan_Wood

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2227 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Access Expert Reader Troubleshooting

Admiral Alan_Wood Admiral
‎2022-11-22 02:55 PM

Issue

Steps for Troubleshooting Readers

Product Line

EcoStruxure Access Expert

Environment

Access Expert Hosted V3

Cause

Readers are offline or not returning the correct card data

Resolution

Common Issues

Issue Solution
My reader is not returning any data when I present a card

Check to make sure the technology card you are using matches the requirements of the card reader. A prox card will not work on an iClass reader.

Check the Reader wiring to confirm CLK and DATA on wired correctly.

Check that the Reader addressing matches the reader port.

Check the power being supplied to the reader. Multiclass readers cannot be powered off S2 (green boards). They require an external power supply.

Bluetooth readers cannot be powered off the S2 (green) boards. The power required by the Bluetooth readers is directly related to the range at which the Bluetooth readers are programmed to work.

My reader is returning different results every time I swipe my card. Check the power to the reader. If the reader requires more power than the board can provide, use a dedicated power supply.
My reader is returning the correct number of bits but the encoded card information is incorrect. Check to make sure your CLK and DATA wires are not switched. If the CLK and DATA wires are switched the 0's and 1's will be inverted causing the card number reported to be wrong. 
My reader is returning the correct number of bits but the raw HEX data is all 0's.  This is most often caused by a bad reader or a bad port on the Mercury board. Check the reader wiring and power first, then try the reader on a different port. 
 
My EP1501 uses the Reader 1 port for my SIO, how do I utilize the on-board reader? The on-board reader for the EP1501 is placed on the internal port and is physically placed on Reader 2 (TB3); it should still be addressed as reader address '0' in Feenics.
I wired my reader to Reader 1 on the board, what's my reader address?

All reader addresses are -1 from the physical port the reader is wired to. Reader wired into Reader 1 is address 0.

I don't understand what to set my offline access method to.

No Change: Reader access will remain in the 'Online Access Method'.

Facility Code Only: Only the facility code is required to receive and access granted event.

Unlock: The reader will unlock during its offline state.

Lock Down: The reader will be locked down during its offline state.

OSDP Reader goes offline when I select 'Secure Channel'.

From the top menu bar select 'Start Linking Mode'. The OSDP reader will come back online.

Please Note: The OSDP reader must be new or never have been configured for Secure Channel previously. If it was previously configured for Secure Channel it will need to be reset with a config card.

My Engage NDE/LE lock is showing a Magnetic Tamper Follow the manufacturers instructions to calibrate the door sensor.
My reader is posting "Access Granted - Not Used" events. This can happen for two reasons.
First, the cardholder badged at the door but never opened the door to enter.

Second, the door does not have a door contact wired at the door and one is programmed into the system. Since there is no device telling the system if the door was used, the system reports no door use.
My reader is posting "Access Denied" events immediately after "Access Granted" events.

Whenever troubleshooting event data always be sure to expand the event message to learn more.

If the event is returning data is without a card read following the first access event, it suggests there may be power coming back into the comms, or are sending feedback into the comms loop.

You can test this by

  1. Does removing the load (pull the output/strike) oof the terminal render the same results?
  2. Is there any change when placing the reader directly onto the Mercury board?

A thorough investigation of the power wiring on the board will help isolate the location of the issue.

My reader is posting "Access Denied - Incomplete Card or PIN Sequence"

The Card and PIN reader mode requires a valid PIN sequence followed by a valid card read.

The Incomplete Card or PIN Sequence can occur

  1. Only the card was presented to the reader.
  2. Only the PIN Code was entered at the reader.
  3. The card was presented before the PIN code was entered.

Keep in mind, if someone enters a random PIN sequence at a reader and happens to guess a valid PIN but does not present a card, this event will show.

The reader is producing an "Unidentified Person on Site" event.

This event is produced when a controller grants access at a reader to a cardholder that is on the controller database, but that is not currently within the Feenics Database. This can happen if a controller missed an event when a person was deleted from the database. The system will delete this card from the controller after this event. The next step is to identify the person and remove them from the building.

The reader is posting "Access Denied - Invalid Facility Code" but showing the correct Facility Code in the expanded event data.

This can occur if the Card Format programmed with the appropriate Facility Code on the controller does not have the correct parity bits for the card being used.

The Mercury Service checks the Card number, the Facility Code, and the parity bits in that order. Due to this, when creating a card format, the parity bit is often the last part of the Card Format to be checked.

Access Denied - Card/Pin Not Found

The User does not have access to the door. Add the User to the door through an Access Level

 

 

Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (9)
  • Find more articles tagged with:
  • Access Expert
  • AlanWood22
  • AlanWood23
  • data
  • incorrect
  • offline
  • reader
  • readers
  • troubleshooting
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.