Access Expert Elevator Access Levels

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Access Expert Elevator Access Levels
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Alan_Wood
    Alan_Wood

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
983 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Access Expert Elevator Access Levels

Admiral Alan_Wood Admiral
‎2022-10-19 05:27 PM

on ‎2022-10-19 05:27 PM

 


Issue

Access Expert Information is needed for Elevator Access Levels

Product Line

EcoStruxure Access Expert

Environment

Access Expert V3 Hosted

Cause

Access Expert Elevator Access Level configuration information 

Resolution

Overview

The Elevator Access Levels are used to determine when a person can access certain floors. Floors can be assigned scheduled access within the Elevator Access Level to determine what floors a person has permissions to gain access to.

 

Elevator Access Levels

Elevator Access Levels use the same Schedules as other aspects of the Keep system. Floors can be added by individual numbers or by groups of numbers with a “-“ between them.

 It is important to note that People are not added to the Elevator Access Level. People are added to the Access Level for either traditional reader-controlled points such as doors or gates while at the same time being granted access to the reader controlling elevator access. This approach means that management of where and when a person can go places can all be controlled from one page.

 

Creating Elevator Access Levels

To create a new Elevator Access Level:

  1. Select the ‘Access Configuration’ tab.
  2. Choose the “Elevator Access” button From the menu.
  3. Click “Add Elevator Access Level”.
  4. Enter a Display Name.
  5. (OPTIONAL) Select a Default Reader Mapping.
  6. Select “Add Elevator Floor Entry”.
  7. Select a Schedule.
  8. Enter the desired Floor Numbers.
  9. Click “Save” or “Save & Close”.
 

The Default Reader Mapping will apply the floor names assigned at the Elevator Reading Page to all readers that use the Elevator Access Level. This also allows for the selection of floors for the Elevator Access Level based on the named floors.

 

To Assign an Elevator Access Level:

  1. Select the ‘Access Configuration’ tab.
  2. Select “Access Levels” from the Menu.
  3. Open the desired Access Level.
  4. Select “View Elevator Access”.
  5. Click “Add Elevator Access Level Entry”.
  6. Choose an Elevator Access Level & associated Elevator Reader. 
  7. Click “Save” or “Save & Close”.
 

It is important to note the flow of the different type of Access Levels:

  1. Elevator Access Levels are applied to Access Levels.
  2. Access Levels are applied to People.
Labels (1)
Labels:
  • EcoStruxure Access Expert
Tags (5)
  • Find more articles tagged with:
  • Access Expert
  • access levels
  • AlanWood22
  • configuration
  • elevator
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.