- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-11-22 05:19 PM
Zelio Soft 2 5.4.2 Boolean Parameter Window Output Column not showing
Hi there,
I'm having a problem using the boolean function. I was using a software version older than this one with the same problem, I thougt if I could install a recent version the problem will go away, but it still remains. The problem is the following:
When I use a boolean function and I open the parameters window, every column of the inputs is correctly visualized but the output column that is partially visualized (See the attached image). The parameters window don't let change the size and neither the columns of the inputs let change the width, so I can't see when the outputs values are set to 0 or 1. I suppose that the problem is with the computer, but I want to listen what the community think about it. Thanks in advance,
Ernesto.
- Tags:
- english
Link copied. Please paste this link to share this article on your social media post.