Posted: 2024-11-02 01:20 AM
MICOM C264
Reference to the device (Micom C264-IAVR) we need to edit setting from HMI , but the parameters are not appears in HMI so we moved to connect with software
- The following steps have been applied:
1- Name of device: C264S11M6A10013022000001111DT0
2-we install this programs (CAT-MICOM S1 Pacis - SCE .)
3-Connect the laptop to the C264-IAVR via an Ethernet connection.
4-Open (CAT software and create a new connection with the device using the ( refresh button)
5-Connect to the device and enter profile: Engineer,
password: AAAAAAA
6-Put the device in BOOT mode And apply the steps as mentioned in the manual from page962 to page 999
7-must be send A DATA BASE and sent to the C264.
- Inquiries:
We have applied all steps from 1 → 6 and stopped at step number 7.
- where can i find the database to upload for this device?
- if i did not applied step number 6 and i want to create new setting file by micom s1 pacis, i will open micom s1 pacis then go to this path (open - setting file -there is not response ) so how can matter be solution? .
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
Posted: 2024-11-04 11:08 AM
Hi,
C264-iAVR is a particular application of the C264, the device is already loaded with the right firmware.
The user can configure the device simply through the webHMI by connecting to the device through a web browser.
The described procedure is meant to be applied to C264 to load the firmware and database compatible with the system where it is installed.
I fear the internal firmware has been erased.
I would invite you to contact your local technical support that will assist you.
https://www.se.com/ww/en/work/support/country-selector/contact-us.jsp
Link copied. Please paste this link to share this article on your social media post.