Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

When I am using a serial to ethernet converter, how should I configure MatrikonOPC Server for SCADA Modbus?

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.
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
  • Industrial Automation
  • AVEVA Plant SCADA Forum
  • When I am using a serial to ethernet converter, how should I configure MatrikonOPC Server for SCADA Modbus?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
olivier_vallee
Commander olivier_vallee
34
Oncom
Commander Oncom
6
Kien_Mac
Lieutenant JG Kien_Mac Lieutenant JG
2
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to AVEVA Plant SCADA Forum
Start a Topic
Anonymous user
Not applicable

Posted: ‎2020-07-07 03:05 AM

1 Like
3
4670
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
Posted: ‎2020-07-07 03:05 AM

When I am using a serial to ethernet converter, how should I configure MatrikonOPC Server for SCADA Modbus?

Serial to Ethernet converters can come in different varieties.

 

Serial to Ethernet Connector that allows you to work with Modbus to Ethernet. It enables you to provide shared access to a local Modbus device over network, so other network users can reach its content and functionality as if it were attached directly to their machines. In a similar way, you too can access a remote Modbus over Ethernet regardless your physical proximity to the device. 

Some converters, such as Lantronix, will simply receive serial data, encapsulate it in a TCP packet and send it to the desired IP address.  In this case, the underlying Modbus protocol is still the serial "Modbus RTU" or "Modbus ASCII". You will want to use the "0 RTU (CRC16)" or "1 ASCII (LRC)" format in your Modbus Unit configuration for the MatrikonOPC Server for SCADA Modbus. If you are using the MatrikonOPC Server for Modbus (non SCADA) you will want to use the "TCP/IP Terminal Server".

Some converters, such as Moxa and Garretcom, will go one step further and convert the Modbus protocol from Modbus RTU to Modbus TCP. This is useful in cases where multiple masters, such as redundant OPC servers, need to access the data. Modbus TCP differs from Modbus RTU, in that its messages do not use a CRC/LRC, and each message is prefixed with a 6-byte header. Make sure you choose the format "2 RTU TCP" in the Modbus Unit. If you are using the MatrikonOPC Server for Modbus (non SCADA) you will want to use the "Modbus Ethernet PLC (TCP/IP)".

 

  • Tags:
  • com port
  • english
  • modbus
  • scada
  • serial port
  • serial to ethernet converter
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
Rodrigo_Garcia
Commander Rodrigo_Garcia Commander
Commander

Posted: ‎2020-07-20 06:55 AM

1 Like
2
4633
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
Posted: ‎2020-07-20 06:55 AM

Thanks for sharing!

Rodrigo G. 


Industrial Automation Community manager

  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

RoozeeR
Lt. Commander RoozeeR Lt. Commander
Lt. Commander

Posted: ‎2020-07-20 08:22 AM

In response to Rodrigo_Garcia
3 Likes
1
4630
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
Posted: ‎2020-07-20 08:22 AM

You have to define the IP address of the Serial to Ethernet converter and the Modbus address. The Modbus address depends on how your converter is configured. When it's configured to have Modbus slave(s) connected, the Modbus address = Modbus address of the slave. Be aware that you set your OPC request speed at a level that can be handled by the converter and your Modbus device.

 

Capture.GIF

When it's configured to have a specific slave connected, the Modbus address of the slave is probably defined in the converter. You should read the converters manual how to address the slave.

When a Modbus Master is connected to the converter, your OPC server should be able to receive (unsolicited) data form the converter. I'm not sure if Matrikon OPC can do this.

R.Roozee
Sr Solution Architect (SAE Master)
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

BevanWeiss
Spock BevanWeiss
Spock

Posted: ‎2020-07-22 08:21 PM

In response to RoozeeR
0 Likes
0
4614
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
Posted: ‎2020-07-22 08:21 PM

There really are so many different ways to do this...

Some vendors (such as Schneider) provide ModbusTCP to ModbusRTU gateways.

Others like Perle / Moxa can also provide just pure serial<->ethernet converters with various features available.

 

I know that both Perle / Moxa have a driver that can be installed which can enable the converter to appear identical to a local serial port, down to DCD/CTS/DTR/RI (modem signal) emulation and all.. Moxa call this RealPort I believe.

In such a mode, it's possible to use it on a multidrop RS485 network (with multiple ModbusRTU masters if required).. the likes of Kepware / Matrikon typically support these just fine.

 

When using the RawTCP (aka Telnet) mode, then you just setup a straight TCP socket (often it can be configured who will be the initiator) and then bytes received on the serial port will just be sent across the TCP socket, and bytes received on the TCP socket will be transmitted out the serial port.  Typically in this mode you lose the flexibility of dynamic changes to baud rate, or modem signal support, but you also have less software layers involved, so fault finding can be easier.

 

I think it is all about horses for courses... certain situations will exhibit a preference for one solution over another.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.