Adding a New Citect SCADA Station with Fewer Pages (Compatibility with Existing Project & Licensing)

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.
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
  • Industrial Automation
  • AVEVA Plant SCADA Forum
  • Adding a New Citect SCADA Station with Fewer Pages (Compatibility with Existing Project & Licensing)
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
olivier_vallee
Commander olivier_vallee
34
Oncom
Commander Oncom
6
Kien_Mac
Lieutenant JG Kien_Mac Lieutenant JG
2
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to AVEVA Plant SCADA Forum
Start a Topic
Anonymous2235
Anonymous2235
Cadet

Posted: ‎2025-06-01 09:18 AM

0 Likes
1
314
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
Posted: ‎2025-06-01 09:18 AM

Adding a New Citect SCADA Station with Fewer Pages (Compatibility with Existing Project & Licensing)

If I would like to set up a new Citect SCADA station based on an existing project (Citect 2018 R2). The new station will use the same I/O tags and data source but will have fewer graphic pages—so it needs to be a separate project file with some pages removed.

Here are my concerns:

  1. Is it possible to run two Citect project files (the original and the trimmed-down version) while sharing the same I/O server and tags?

  2. The only available client licenses are for Citect 2023. Can a 2023 runtime client license work with a project developed in Citect 2018 R2?

Any insights or best practices would be greatly appreciated.

Labels
  • Labels:
  • Plant SCADA Runtime
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
olivier_vallee
Commander olivier_vallee
Commander

Posted: ‎2025-06-03 02:09 PM

0 Likes
0
290
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
Posted: ‎2025-06-03 02:09 PM

Hi @Anonymous2235 

To answer our questions,

1. Yes, it is possible to run a cut down project while sharing the same IO and tags. The main project (call it the server) will need to be defined in the project. Then on the client project, this same project, but with reduced pages. The use of "Include Projects" can help facilitate this and make maintenance of the project easier (think of an include project as a container for certain config).

2. Yes, a 2023 runtime license can work with an older product version, as long as that license type existed in that previous version (Sentinel USB is the most common and widely supported).
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.